This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS100BR210: Does DS100BR210 support the SMPTE 292?

Part Number: DS100BR210
Other Parts Discussed in Thread: LMH1218, LMH1219,

Hello,

In our application, we need to support both SMPTE 292 video input and output. So we plan to use both LMH1219 and LMH1218 for this application. The FPGA and the LMH1218 / LMH1219 are located on a separate card. So the diff pairs from FPGA' SerDes will be routed through the backplane card then to the LMH1219 / LMH1218 via several connectors.

Can I use the DS100BR210 to re-drive the signals from an FPGA' SerDes Rx/Tx then feed them to the LMH1218 / LMH1219 for SMPTE 292? 

Thanks in advance!