Part Number: SN65DSI86
Hi TI,
We have few unit which are having screen blank problem after boot or when the device enter into sleep state. I have pulled the register dump from failing unit and listed below. Also we found that 0x96 reg is 0x0 (main link off) when the issue happened. In our SW we are setting 0x96 reg to 0xA (fast link training) but when the issue occurs we are getting 0x0 from the edp bridge chip. Can you help us debug this issue? Device kernel log showing "Link training failed and link is off".
| F0 | 0x00 |
| F1 | 0x00 |
| F2 | 0x00 |
| F3 | 0x00 |
| F4 | 0x01 |
| F5 | 0x02 |
| F6 | 0x00 |
| F7 | 0x00 |
| F8 | 0x06 |
| F9 | 0x00 |
| FA | 0x00 |
| FB | 0x00 |
| FC | 0x00 |
| FD | 0x00 |
| FE | 0x00 |
| FF | 0x00 |
Thanks
Mani