This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65LVDT33: IBIS model shows the max differential input voltage violating datasheet spec

Part Number: SN65LVDT33
Other Parts Discussed in Thread: SN65LVDS33

Team, 

Working on simulating a design and The simulation using the SN65LVDT33 part shows the max differential input voltage of ~860-930mV peak-to-peak, which is violating the datasheet requirement, VID=800mV.  It seems the SN65LVDT33 has a tight input differential voltage requirement... For this case, do you recommend using the SN65LVDS33 part with the external diff termination instead? Or do you have any other recommendations?

The IBIS model found in the product page didn’t include the termination resistor so simulation was done with added 110ohm differential termination in the model