I have a customer with the following questions:
1) Does the TUSB9261 support port multipliers and/or FIS-switching on its SATA port?
I have tried interfacing the TUSB9261 eval board with 2 different port multipliers but so far have had no success getting multiple drives to work (the port multiplier will only function as a single drive pass-through).
2) Has TI tested the TUSB9261 with Intel's ICH9M IO controller?
I have tried the TUSB9261 eval board with two different single board computers that each use the ICH9M IO Controller for the USB port.
Neither enumerate the TUSB9261. The board functions fine when I use it with the USB ports (USB 2.0 and USB3.0) of the desktop PC at my desk (which I'm sure has a different IO controller supplying the USB ports).
Thanks,
Rinzai Bell