Other Parts Discussed in Thread: TLK10232
Hello
Team
TLK10232_AN.pdf (SLLA351) For the description, please tell me.
■ References
TLK10232_AN.pdf (SLLA351)
1.2 What Happens When Link Training is Activated? (page2)
---------------
Registers 0x9012 and 0x9022 are 16-bit registers, but only the lower byte is valid data.
The most significant bit (MSB) of this byte represents the most negative pre cursor value, the least significant bit (LSB) the one for 0%.
The first read register is the most positive POST_CURSOR1 setting.
With every read the POST_CURSOR1 parameter is decreased to the next lower value, ending with the most negative after 32 reads.
The bit patterns and corresponding POST_CURSOR values can be looked up from Table 5 on page Error! Bookmark not defined ..
---------------
★ Question 1
Following contents are described in Section 1.2 (page2) for (0x01.9022 register), I would like a detailed description.
Thank I need your help.