Part Number: SN65DP149
there is no AUX_P/N in DP149 and just confirm GPU's AUXp/N connecting to SDA_SRC and SCL_SRC of DP149 with 2K pullup to 3.3V .
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65DP149
there is no AUX_P/N in DP149 and just confirm GPU's AUXp/N connecting to SDA_SRC and SCL_SRC of DP149 with 2K pullup to 3.3V .
Hi Peter,
GPU's AUX will connect to DP149's DDC ports.
I need to confirm if we recommend using DDC snoop mode in this device.
Regards
Hi Peter,
DDC is display data channel it uses I2C(SCL/SDA)
If the GPU only has AUX port, this port may send I2C compliant levels or I2C-over-AUX when CAD=H.
DP149 implement clock stretching, if you face interoperability issues you would have to implement DDC snoop mode
DP159 includes an I2c-over-AUX to DDC level shifter.
Regards