This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ron
Thanks for your reply.
system 1 is old, and I can not change it.
system 2 has only 1 input with 2 pins in the connector C_P, C_N. in RS422 format.
So, I need to design a "box" with a fuction that do a logic OR between the 2 signals.
I need that it will be simple and low cost.
I want to use:
A. wired OR between the positive A_P OR B_N => C_P
B. wired AND between the negative A_N AND B_N => C_N
to get new signal in RS422 format.
Is it possible?
do I need the GND from the system 1 ?
waiting to your reply.
Haim