Other Parts Discussed in Thread: TPD7S019, TPD12S520, TPD12S521
Is the TPD7S019 a recommended part for VGA ESD protection for output port?
Is there an equivalent for the VGA input port?
Are tjeTPD12S520/521 recommended for HDMI in/output ports?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TPD7S019 is for VGA output port only. If using it for an input port, while the VLT's would translate back down, the system side of TPD7S019 would have to connect to the connector, and TPD7S019 does not provide ESD protection on the system side.
TPD12S520 is for HDMI input (receiver) port.
TPD12S521 is for HDMI output (transmitter) port.