Other Parts Discussed in Thread: DP83848VYB, TM4C129XNCZAD
Hello,
i didn´t get the DP83848VYB on my self-designed board with an MPC5566 processor working.
Here are the Register values of my PHY:
BMCR: 0x3100
BMSR: 0x7849 (no link)
PHYSTS: 0x4000
PHYCR: 0x0804
The Board is connected to my Windows 7 PC but the auto-negotation will never be finished and also couldn´t the PHY establish a link.
Here are some values I measured on the PHY:
TX_CLK: 25Mhz
TX_EN: HIGH when transmitting on TXD_0/1/2
X1: 25Mhz
X2: not connected
25MHZ_OUT: 25Mhz
RESET_N: HIGH (low active)
MII_MODE: LOW
3.3V supply: 3.3V
PFB(IN/OUT): 1.8V
Resistance RBIAS to ground: 4.87 kOhm (from circuit layout)
Resistance TD/RD to termination: 50 Ohm (from circuit layout)
MDC: while reading register: 25Mhz; after reading no clock at 0V
I also tried it with a fixed 100Mbit/FullDuplex and 10Mbit/FullDuplex configuration but there also couldn´t be a link established.
Hope anybody can help be to solve this problem!
Thanks!
Best regards,
Stefan