This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867IRPAPT High Immunity 10/100/1000 1.8V - VIL issue

 DC analysis of DP83867IRPAPT High Immunity 10/100/1000 Ethernet Physical Layer Transceiver and ZYNQ XC7Z030-1FBG676I.

But we found DC analysis error between them, please go through it and let us know any solutions or we can go ahead with design.

3323.DC-Char_Issue.pdf

Zynq VoL is 450mV and PHY Vil is 360 mV.

1. Is it compatible ?

2. If it is no issue, PHY is under go  temperature test at -45 deg C to + 85 deg C, will support the same?

Kindly give your suggestion.

Thanks and regards,

Veeranarayanan R

  • Hi Veeranarayanan,

    1. Yes they are compatible. The DP83867 can support Vil up to 0.45V.
    a. The DC spec issue mainly arises from how Xilinx specs the driver at guaranteed iol = 8mA. Xilinx suggests using IBIS models to determine what actual Vol will be. See a related thread: forums.xilinx.com/.../427880

    2. Yes the the Vil will be 0.45V across the operating temperature range: -40C to 85C

    Best Regards,