This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83640 100BASE-FX PMD Input Threshold



Hi!

Does anyone know what is the thresholds for the 100BASE-FX PMD input pair? The datasheet indicated that it is PECL implementation but I am thinking it should be LVPECL to be exact. Either way, the thresholds for the data input pair are not listed. The PMD output pair is listed as 0.3V-0.93V. I am assuming there will be a minimum threshold for the PMD input pair.

Thanks,

SH

  • Hello,

    The fiber transmit and receive pins are differential and are designed to be LVPECL compatible.  In the case of the fiber transmit specification, the minimum output levels from the device should be 0.3V single-ended, 0.6V differential.  This signaling should meet the requirements of the fiber transceiver inputs.  Typically, the transmit signaling will be closer to 0.5V single-ended, 1.0V differential. 

    Thanks,

    John

  • John,

    Thank you for the reply. I am also trying to make sure that the tranceiver signaling will meet the Ethernet Phy as well. I took some measurement and the tranceiver is sending at around 1.3-1.4V pk-to-pk. What is the minimum threshold for the Eth Phy INPUT?

    Thanks,

    SH

  • In 100Base-FX mode, the RD+/- pins are designed to accept LVPECL voltage levels.  The signals would nominally be 800mV (single ended). 

    Based on the results of our device characterization, the RD+/- pins should be able to accommodate signaling of 1.3 - 1.4 Vpp (differential) with some margin.  These signal levels should not pose any problems.

    Patrick