Hello ,
I am using PCA9548 as I2C mux in my design, to connect Upstream I2C from a 3.3V device to a 2.5V down stream device.
Is it possible to provide a pull up of 3.3V on upstream I2C ,and connect the down stream I2C to a 2.5V device with a pull up of 2.5V?
Need to make sure that the voltage level on the 2.5V device I2C depends just on the pull up provided in the downstream I2c signal and does not depend on the upstream pull up.
Will PCA9548 act as a voltage translator? so that the 3.3V pullup on Upstream I2C will not damage the 2.5V device on the down stream.