Other Parts Discussed in Thread: DS80PCI810
Hello,
I would like to ask the "RXDET" functions for DS80PCI810.
According to the DataSheet.
When it is in "F" mode.
PCIe detection occurs; termination is Hi-Z until Rx detection; once detected input termination is 50 Ω
Q1: What is the input termination is Hi-Z?
Q2: What is the input termination is in 50 Ohm?
And
Q3: Where does the RX begin to detect?
The input termination part means Re-driver's TX or Re-driver's RX side?
Thanks a lot.