Hi,
one of my customers is asking what should be the voltage of Vbat if Vdd33 is shorted to Vbat externally. He is confused because we suggest different voltages on the DS:
1. first we say that Vbat shouldn't be under 3.3V
2. then we say that Vbat min is 3.05V
3. And we also give the following range for Vbat 3.2-3.6V
Which would be the recommended voltage for Vbat, and why are several different voltages recommended?
What would be the recommended voltage for Vbat when Vdd33 is supplied by the internal LDO?
thanks,
Tadeo