Hi,
datasheet states that "When operating in 3 supply mode, the 2.5-V VDDA2P5 can come up with or after the 1.8-V VDDA1P8 but not
before it." and troubleshooting guide reads "the VDDA1P8 supply must be stable within 25ms of the VDDA2P5 supply ramping up". If i understand correctly, the later means that 2P5 allowed to ramp up before 1P8 which contradicts to datasheet. Also troubleshooting guide requires foe 1P8 to be shut down before 2P5 on powering down while DS omits powerdown case.
Could you please tell the correct powerup/powerdown sequence and whether it is critical at all in case all 3 supplies ramp up within 15 ms from first to last?
TIA
Sergey