Part Number: SN65HVD3082E
Good day Colleagues,
Could you tell me about a total power consumption of the SN65HVD3082E for 100kBit/sec data rate and 256 loads? Termination is 60 Ohm.
Am I correct the total current will be 35 mA + 8 mA = 43mA (figures 5 and 2 from the datasheet)?
Datasheet also says, the output current can be up to 60mA, but I can't understand for what condition 60mA can flow to the output?
Customer has only 85mA of the current to supply the transceiver for RS-485 and worries it will be not enough.
Thank you, Mike