Part Number: TUSB9261
I'm trying to implement ATA Pass-Through commands for the TUSB9261DEMO board based on the SCSI/ATA Translation - 4 (SAT-4) document (revision 05 from 11 March 2016). According to this specification document all devices supporting ATA Pass-Through commands shall support the ATA Status Return descriptor. Based on my testing so far, the demo board supports ATA Pass-Through (12 and 16) commands, but does not appear to support the ATA Status Return descriptor. Can you confirm if the ATA Status Return descriptor should be supported? Note, our demo board is running firmware v1.05.