Part Number: MAX3232
Other Parts Discussed in Thread: MAX232
Hello:
We are using some MAX3232 in a project, we use like with suggested components showed in datasheet diagram, we are using T2 and R2 channels (7,8,9 and 10 pin) if we power MAX232 and them connect to RS232 device, systems works fine, and power current is about 0.5 mA, all OK, but if we connect RS232 device and them we power max 3232, power current is about 400 mA and doesn't work.
System only works if we first power MAX3232 and after we connect to RS232.
We tryied connecting not used channel inputs (11 and 13 pins) to ground or VCC like explained in datasheet, but doesn't work. We tryied with some different MAX3232 units.
¿What's the problem?
Best regards.