Part Number: TMDS181
Hi team,
I using TMDS181 have problems in doing HDMI certification.
test result as below:
The former is the result of hardware control and the latter is the result of software control.
There are obvious differences. Now there are problems in HDMI certification. I don't know where there are differences.
Now the problem is that there is a problem with eye diagram in hardware control.
In software control, eye diagram OK but it can't pass 2 items of 1-1 and 1-4 fold. In hardware control, 1-1 and 1-4 items are OK.
the HDMI 1-1 and 1-4 test items as below:
the circuit as below:
need help to solve this issue.
thanks,