This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB921-Q1: Multiple Input formats and Sync Polarity

Part Number: DS90UB921-Q1
Other Parts Discussed in Thread: DS90UB940-Q1

Hi,

I want to use the DS90UB921-Q1 serializer and the DS90UB940-Q1 deserializer to take either 16-bit YCbCr parallel CMOS data or 24-bit RGB888 parallel CMOS data send it over FPD-Link III and convert it to a 2-lane MIPI CSI-2 output without changing the physical interface (by just only adjusting the camera settings).

1) Is this possible to do?

The HS and VS signals are active on low and the Data valid signal is active on high.

2) Does the polarity of these signals have any effect on whether or not it can be connected to the input video control pins of the ser?

Thank you,

JP