This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB954-Q1: Can DS90UB954-Q1 process two different resolutions simultaneously?

Part Number: DS90UB954-Q1


Hi,

I currently have the following applications:

DS90UB954 has two different resolutions. 60 FPS with the same true number

But there are two different resolution assumptions: 1 million and 2 million.

I wonder if this chip can be used in this way.

Thanks.

  • Hello Wu,

    Do you me to be connected to two Serializers and Imagers having different resolutions? Or just one Imager having two different streams?
  • Hi Hamzeh,

                         I mean connected two camera, it have different resolutions.

                        could ds90ub954-Q1 support this application?

                         btw, if FPS also different, ds90ub954-Q1 could support this application?

    thanks,

  • Yes, the 954 can be paired with different cameras having different resolutions and FPS.
    In this case you need to use the Best-Effort Round Robin CSI-2 Forwarding Mode where each image sensor is assigned a VC-ID to identify the source. Different data types within a virtual channel is also supported in this mode.