Part Number: DS90UB933-Q1
Hi Sir,
1. Due to the current input inquiry is 8 bit Parallel 8 bit input, how to do the DIN[0, ,11] of DS90UB933-Q1 and shematic is better for such application limitation.
2. How to do control in such condition?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB933-Q1
Hi Sir,
1. Due to the current input inquiry is 8 bit Parallel 8 bit input, how to do the DIN[0, ,11] of DS90UB933-Q1 and shematic is better for such application limitation.
2. How to do control in such condition?
Hello Ja,
Please use 10 bit mode and connect only the lower 8 inputs or the upper 8 inputs. Either configuration is ok. The deserializer can be configured to recognize either the lower 8 bits of upper 8 bits.
Best Regards,
Casey
Hi Sir,
Would you please help to advise the following:
The Data pin in which did not use in such 8 bit mode, how you advise: Connecting to high potential or connecting DGND?
Ja