Part Number: DP83822I
To the person concerned
Regarding strapping related pins on DP83822, I have question.
At pin fuction table, I found below notice relevant to strapping pins
"f) Type: S-PU, S-PD - Strapping Pin (All strap pins have weak internal pullups or pulldowns. If the default strap value is needed to be changed then an external 2.2-kΩ resistor should be used)
In order to make intended operation , Datasheet recommends to apply 4-Level bootstrap and specifies PD or PU resistor values for each of 4-Level cases.
qustion is that what happen if external 2.2-kΩ resistor is co-existed with resistor matrix for 4-level strapping.
For example, in case of BOOSTXL-ETHERCAT reference circuit, external 2.2-kΩ resistors are existed on pins for the strapping. if customer adds another external resistor for 4-Level strapping, What kind of problem can be coming?
in addition, Could you explain when external 2.2-kΩ resistor is needed?
thank you
Best Regards
Mark Kim