Part Number: DS90UB960-Q1
Hi all,
I have following setup: TDA2p -> UB960 -> Coax -> UB953 -> IMX390 sensor.
I'm receiving frames from camera without any problem (FULL HD, 60 fps), but I have some strange problems related to I2C communication with sensor.
In run-time, exposure parameters are set for every frame via I2C. The problem I'm facing is that sometimes I2C write fails (every few minutes):
[HOST] [IPU2 ] 205.169706 s: src/bsp_deviceI2c.c @ Line 1271:
[HOST] [IPU2 ] 205.169859 s: I2C2: DEV 0x44: WR 0x0008 = 0x0001 ... ERROR !!!
[HOST] [IPU2 ] 205.169981 s: src/bsp_deviceI2c.c @ Line 1293:
[HOST] [IPU2 ] 205.170072 s: I2C2: Error timeout 236 ms!!!
[HOST] [IPU2 ] 205.170682 s: Fail to set sensor aewb data: status=-21!
I suppose this problem could be related to I2C timing parameters, so I have few questions for you:
1. If I have a good understanding, in this situation, UB953 is master proxy and UB960 is a slave proxy?
2. The proxy master (UB953) timing parameters are based on the internal reference clock? Is this correct for synchronous mode?
3. If UB960 is slave proxy, it's not necessary to set I2C timing parameters for deserializer?
4. Could it be related to I2C clock stretching? I noticed following - If I set BCC_WATCHDOG_TIMER value from BCC_WATCHDOG_CONTROL register to 0x01 instead of 0x7F, timeout from error above will be 1-2 ms, instead of 236 ms.
I would appreciate some advice or help with this issue.
Best regards,
Stefan.