Part Number: DP83822IF
Hi team,
My customer is trying to connect media-side to 100BASE-FX and use LED_1/GPIO1 as signal detect.
Could you please help me answer my customer's questions below?
1. Is the input signal supposed to follow Table 7.5 VDDIO VIH/VIL level? My customer wants to double check it because other vendors defines that it Signal Detect follows LVPECL.
2. DS p.40 8.4.4.2 recommends to use Signal Detect when 100BASE-FX. What is the disadvantage of not using Signal Detect here?
3. About the statement below:
if the electrical link between the fiber module and the DP83822 is broken, disconnected or otherwise disrupted, the link will recover only by initiating a soft reset through MDIO/MDC interface.
Does the Signal Detect continue to detect under the condition that the optical fiber is disconnected? My customer cares about that because it may need soft reset.
Regards,
Itoh