Dear TI team,
I would like to share with you one issue which we are having with 954 together with 953 device. We are working with both devices, carrying video stream from two cameras. The cameras work at 2MP each. We are using about 2.5m of coax cable, with two interconnections between. 1.5m is Leoni Dacar 452, and 0.5m part is Leoni Dacar 302.
The point is, that we need to fulfil the ESD test according to our customer, the test is Indirect Discharges (Islands), and we need to be stable till 8kV, the point is that at 7kV, we have flickering in the image, and we have checked that we are loosing the lock between the 953 and 954. Our system is properly shielded, and it seems the problem is not the discharge itself, is the radiation which is created because of the discharge. (We already have TVS protection diode in the FPDLink line)
We are working in COAX mode and the voltage is 10V.
Do you have any recommendation to avoid to have this undesired flickering? Is not completely loss of the image, it looks, only image moved, strange artefacts.... If you need any further information, please tell me.
Thanks and regards!