Part Number: TCAN4550
Hi Team,
The customer is experiencing below issue and needs your help. He obtained the tcan4x5x driver from the linux-5.14 version, and found the following problems during debugging:
- When the device driver reads the ID as a match, it calls tcan4x5x_read_reg. This function adds 0x1000 to all address offsets in the address bit, and the send address data is 0x41100001. According to the manual, it should be 0x41000001. It is normal to read ID after modification;
- According to the logic judgment after reading the ID in m_can_check_core_release (), the ID of the read ID0 should be 0x4e414354 according to the manual and the actual measurement result. But it can not meet the 30-32 judgment logic of the later version judgment. The customer speculates whether to read the value of ID1 0x30353534, and the subsequent logical judgment is 30, which conforms to the judgment of the later version;
- After the modified part of the driver can be loaded normally, it can be called in the application layer socket after the successful loading of the can device. Application write prompt "No buffer space available";
- spi is big-endian transmission (spi problem), the chip does not respond, and the response is normal after modification;
Problem 3 is currently unresolved.
// SPDX-License-Identifier: GPL-2.0
// SPI to CAN driver for the Texas Instruments TCAN4x5x
// Copyright (C) 2018-19 Texas Instruments Incorporated - http://www.ti.com/
#include <linux/regmap.h>
#include <linux/spi/spi.h>
#include <linux/regulator/consumer.h>
#include <linux/gpio/consumer.h>
#include "m_can.h"
#define DEVICE_NAME "tcan4x5x"
#define TCAN4X5X_EXT_CLK_DEF 40000000
#define TCAN4X5X_DEV_ID0 0x00
#define TCAN4X5X_DEV_ID1 0x04
#define TCAN4X5X_REV 0x08
#define TCAN4X5X_STATUS 0x0C
#define TCAN4X5X_ERROR_STATUS 0x10
#define TCAN4X5X_CONTROL 0x14
#define TCAN4X5X_CONFIG 0x800
#define TCAN4X5X_TS_PRESCALE 0x804
#define TCAN4X5X_TEST_REG 0x808
#define TCAN4X5X_INT_FLAGS 0x820
#define TCAN4X5X_MCAN_INT_REG 0x824
#define TCAN4X5X_INT_EN 0x830
/* Interrupt bits */
#define TCAN4X5X_CANBUSTERMOPEN_INT_EN BIT(30)
#define TCAN4X5X_CANHCANL_INT_EN BIT(29)
#define TCAN4X5X_CANHBAT_INT_EN BIT(28)
#define TCAN4X5X_CANLGND_INT_EN BIT(27)
#define TCAN4X5X_CANBUSOPEN_INT_EN BIT(26)
#define TCAN4X5X_CANBUSGND_INT_EN BIT(25)
#define TCAN4X5X_CANBUSBAT_INT_EN BIT(24)
#define TCAN4X5X_UVSUP_INT_EN BIT(22)
#define TCAN4X5X_UVIO_INT_EN BIT(21)
#define TCAN4X5X_TSD_INT_EN BIT(19)
#define TCAN4X5X_ECCERR_INT_EN BIT(16)
#define TCAN4X5X_CANINT_INT_EN BIT(15)
#define TCAN4X5X_LWU_INT_EN BIT(14)
#define TCAN4X5X_CANSLNT_INT_EN BIT(10)
#define TCAN4X5X_CANDOM_INT_EN BIT(8)
#define TCAN4X5X_CANBUS_ERR_INT_EN BIT(5)
#define TCAN4X5X_BUS_FAULT BIT(4)
#define TCAN4X5X_MCAN_INT BIT(1)
#define TCAN4X5X_ENABLE_TCAN_INT \
(TCAN4X5X_MCAN_INT | TCAN4X5X_BUS_FAULT | \
TCAN4X5X_CANBUS_ERR_INT_EN | TCAN4X5X_CANINT_INT_EN)
/* MCAN Interrupt bits */
#define TCAN4X5X_MCAN_IR_ARA BIT(29)
#define TCAN4X5X_MCAN_IR_PED BIT(28)
#define TCAN4X5X_MCAN_IR_PEA BIT(27)
#define TCAN4X5X_MCAN_IR_WD BIT(26)
#define TCAN4X5X_MCAN_IR_BO BIT(25)
#define TCAN4X5X_MCAN_IR_EW BIT(24)
#define TCAN4X5X_MCAN_IR_EP BIT(23)
#define TCAN4X5X_MCAN_IR_ELO BIT(22)
#define TCAN4X5X_MCAN_IR_BEU BIT(21)
#define TCAN4X5X_MCAN_IR_BEC BIT(20)
#define TCAN4X5X_MCAN_IR_DRX BIT(19)
#define TCAN4X5X_MCAN_IR_TOO BIT(18)
#define TCAN4X5X_MCAN_IR_MRAF BIT(17)
#define TCAN4X5X_MCAN_IR_TSW BIT(16)
#define TCAN4X5X_MCAN_IR_TEFL BIT(15)
#define TCAN4X5X_MCAN_IR_TEFF BIT(14)
#define TCAN4X5X_MCAN_IR_TEFW BIT(13)
#define TCAN4X5X_MCAN_IR_TEFN BIT(12)
#define TCAN4X5X_MCAN_IR_TFE BIT(11)
#define TCAN4X5X_MCAN_IR_TCF BIT(10)
#define TCAN4X5X_MCAN_IR_TC BIT(9)
#define TCAN4X5X_MCAN_IR_HPM BIT(8)
#define TCAN4X5X_MCAN_IR_RF1L BIT(7)
#define TCAN4X5X_MCAN_IR_RF1F BIT(6)
#define TCAN4X5X_MCAN_IR_RF1W BIT(5)
#define TCAN4X5X_MCAN_IR_RF1N BIT(4)
#define TCAN4X5X_MCAN_IR_RF0L BIT(3)
#define TCAN4X5X_MCAN_IR_RF0F BIT(2)
#define TCAN4X5X_MCAN_IR_RF0W BIT(1)
#define TCAN4X5X_MCAN_IR_RF0N BIT(0)
#define TCAN4X5X_ENABLE_MCAN_INT \
(TCAN4X5X_MCAN_IR_TC | TCAN4X5X_MCAN_IR_RF0N | \
TCAN4X5X_MCAN_IR_RF1N | TCAN4X5X_MCAN_IR_RF0F | \
TCAN4X5X_MCAN_IR_RF1F)
#define TCAN4X5X_MRAM_START 0x8000
#define TCAN4X5X_MCAN_OFFSET 0x1000
#define TCAN4X5X_MAX_REGISTER 0x8fff
#define TCAN4X5X_CLEAR_ALL_INT 0xffffffff
#define TCAN4X5X_SET_ALL_INT 0xffffffff
#define TCAN4X5X_WRITE_CMD (0x61 << 24)
#define TCAN4X5X_READ_CMD (0x41 << 24)
#define TCAN4X5X_MODE_SEL_MASK (BIT(7) | BIT(6))
#define TCAN4X5X_MODE_SLEEP 0x00
#define TCAN4X5X_MODE_STANDBY BIT(6)
#define TCAN4X5X_MODE_NORMAL BIT(7)
#define TCAN4X5X_DISABLE_WAKE_MSK (BIT(31) | BIT(30))
#define TCAN4X5X_DISABLE_INH_MSK BIT(9)
#define TCAN4X5X_SW_RESET BIT(2)
#define TCAN4X5X_MCAN_CONFIGURED BIT(5)
#define TCAN4X5X_WATCHDOG_EN BIT(3)
#define TCAN4X5X_WD_60_MS_TIMER 0
#define TCAN4X5X_WD_600_MS_TIMER BIT(28)
#define TCAN4X5X_WD_3_S_TIMER BIT(29)
#define TCAN4X5X_WD_6_S_TIMER (BIT(28) | BIT(29))
struct tcan4x5x_priv {
struct regmap *regmap;
struct spi_device *spi;
struct m_can_classdev *mcan_dev;
struct gpio_desc *reset_gpio;
struct gpio_desc *device_wake_gpio;
struct gpio_desc *device_state_gpio;
struct regulator *power;
/* Register based ip */
int mram_start;
int reg_offset;
};
static struct can_bittiming_const tcan4x5x_bittiming_const = {
.name = DEVICE_NAME,
.tseg1_min = 2,
.tseg1_max = 31,
.tseg2_min = 2,
.tseg2_max = 16,
.sjw_max = 16,
.brp_min = 1,
.brp_max = 32,
.brp_inc = 1,
};
static struct can_bittiming_const tcan4x5x_data_bittiming_const = {
.name = DEVICE_NAME,
.tseg1_min = 1,
.tseg1_max = 32,
.tseg2_min = 1,
.tseg2_max = 16,
.sjw_max = 16,
.brp_min = 1,
.brp_max = 32,
.brp_inc = 1,
};
static void tcan4x5x_check_wake(struct tcan4x5x_priv *priv)
{
int wake_state = 0;
if (priv->device_state_gpio)
wake_state = gpiod_get_value(priv->device_state_gpio);
if (priv->device_wake_gpio && wake_state) {
gpiod_set_value(priv->device_wake_gpio, 0);
usleep_range(5, 50);
gpiod_set_value(priv->device_wake_gpio, 1);
}
}
static int tcan4x5x_reset(struct tcan4x5x_priv *priv)
{
int ret = 0;
if (priv->reset_gpio) {
gpiod_set_value(priv->reset_gpio, 1);
/* tpulse_width minimum 30us */
usleep_range(30, 100);
gpiod_set_value(priv->reset_gpio, 0);
} else {
ret = regmap_write(priv->regmap, TCAN4X5X_CONFIG,
TCAN4X5X_SW_RESET);
if (ret)
return ret;
}
usleep_range(700, 1000);
return ret;
}
static int regmap_spi_gather_write(void *context, const void *reg,
size_t reg_len, const void *val,
size_t val_len)
{
struct device *dev = context;
struct spi_device *spi = to_spi_device(dev);
struct spi_message m;
u32 addr;
struct spi_transfer t[2] = {
{ .tx_buf = &addr, .len = reg_len, .cs_change = 0,},
{ .tx_buf = val, .len = val_len, },
};
addr = TCAN4X5X_WRITE_CMD | (*((u16 *)reg) << 8) | val_len >> 2;
spi_message_init(&m);
spi_message_add_tail(&t[0], &m);
spi_message_add_tail(&t[1], &m);
return spi_sync(spi, &m);
}
static int tcan4x5x_regmap_write(void *context, const void *data, size_t count)
{
u16 *reg = (u16 *)(data);
const u32 *val = data + 4;
return regmap_spi_gather_write(context, reg, 4, val, count - 4);
}
static int regmap_spi_async_write(void *context,
const void *reg, size_t reg_len,
const void *val, size_t val_len,
struct regmap_async *a)
{
return -ENOTSUPP;
}
static struct regmap_async *regmap_spi_async_alloc(void)
{
return NULL;
}
static int tcan4x5x_regmap_read(void *context,
const void *reg, size_t reg_size,
void *val, size_t val_size)
{
struct device *dev = context;
struct spi_device *spi = to_spi_device(dev);
u32 addr = TCAN4X5X_READ_CMD | (*((u16 *)reg) << 8) | val_size >> 2;
return spi_write_then_read(spi, &addr, reg_size, (u32 *)val, val_size);
}
static struct regmap_bus tcan4x5x_bus = {
.write = tcan4x5x_regmap_write,
.gather_write = regmap_spi_gather_write,
.async_write = regmap_spi_async_write,
.async_alloc = regmap_spi_async_alloc,
.read = tcan4x5x_regmap_read,
.read_flag_mask = 0x00,
.reg_format_endian_default = REGMAP_ENDIAN_NATIVE,
.val_format_endian_default = REGMAP_ENDIAN_NATIVE,
};
static u32 tcan4x5x_read_reg(struct m_can_classdev *cdev, int reg)
{
struct tcan4x5x_priv *priv = cdev->device_data;
u32 val;
regmap_read(priv->regmap, priv->reg_offset + reg, &val);
return val;
}
static u32 tcan4x5x_read_fifo(struct m_can_classdev *cdev, int addr_offset)
{
struct tcan4x5x_priv *priv = cdev->device_data;
u32 val;
regmap_read(priv->regmap, priv->mram_start + addr_offset, &val);
return val;
}
static int tcan4x5x_write_reg(struct m_can_classdev *cdev, int reg, int val)
{
struct tcan4x5x_priv *priv = cdev->device_data;
return regmap_write(priv->regmap, priv->reg_offset + reg, val);
}
static int tcan4x5x_write_fifo(struct m_can_classdev *cdev,
int addr_offset, int val)
{
struct tcan4x5x_priv *priv = cdev->device_data;
return regmap_write(priv->regmap, priv->mram_start + addr_offset, val);
}
static int tcan4x5x_power_enable(struct regulator *reg, int enable)
{
if (IS_ERR_OR_NULL(reg))
return 0;
if (enable)
return regulator_enable(reg);
else
return regulator_disable(reg);
}
static int tcan4x5x_write_tcan_reg(struct m_can_classdev *cdev,
int reg, int val)
{
struct tcan4x5x_priv *priv = cdev->device_data;
return regmap_write(priv->regmap, reg, val);
}
static int tcan4x5x_clear_interrupts(struct m_can_classdev *cdev)
{
int ret;
ret = tcan4x5x_write_tcan_reg(cdev, TCAN4X5X_STATUS,
TCAN4X5X_CLEAR_ALL_INT);
if (ret)
return ret;
ret = tcan4x5x_write_tcan_reg(cdev, TCAN4X5X_MCAN_INT_REG,
TCAN4X5X_ENABLE_MCAN_INT);
if (ret)
return ret;
ret = tcan4x5x_write_tcan_reg(cdev, TCAN4X5X_INT_FLAGS,
TCAN4X5X_CLEAR_ALL_INT);
if (ret)
return ret;
ret = tcan4x5x_write_tcan_reg(cdev, TCAN4X5X_ERROR_STATUS,
TCAN4X5X_CLEAR_ALL_INT);
if (ret)
return ret;
return ret;
}
static int tcan4x5x_init(struct m_can_classdev *cdev)
{
struct tcan4x5x_priv *tcan4x5x = cdev->device_data;
int ret;
tcan4x5x_check_wake(tcan4x5x);
ret = tcan4x5x_clear_interrupts(cdev);
if (ret)
return ret;
ret = tcan4x5x_write_tcan_reg(cdev, TCAN4X5X_INT_EN,
TCAN4X5X_ENABLE_TCAN_INT);
if (ret)
return ret;
ret = regmap_update_bits(tcan4x5x->regmap, TCAN4X5X_CONFIG,
TCAN4X5X_MODE_SEL_MASK, TCAN4X5X_MODE_NORMAL);
if (ret)
return ret;
/* Zero out the MCAN buffers */
m_can_init_ram(cdev);
return ret;
}
static int tcan4x5x_disable_wake(struct m_can_classdev *cdev)
{
struct tcan4x5x_priv *tcan4x5x = cdev->device_data;
return regmap_update_bits(tcan4x5x->regmap, TCAN4X5X_CONFIG,
TCAN4X5X_DISABLE_WAKE_MSK, 0x00);
}
static int tcan4x5x_disable_state(struct m_can_classdev *cdev)
{
struct tcan4x5x_priv *tcan4x5x = cdev->device_data;
return regmap_update_bits(tcan4x5x->regmap, TCAN4X5X_CONFIG,
TCAN4X5X_DISABLE_INH_MSK, 0x01);
}
static int tcan4x5x_parse_config(struct m_can_classdev *cdev)
{
struct tcan4x5x_priv *tcan4x5x = cdev->device_data;
int ret;
tcan4x5x->device_wake_gpio = devm_gpiod_get(cdev->dev, "device-wake",
GPIOD_OUT_HIGH);
if (IS_ERR(tcan4x5x->device_wake_gpio)) {
if (PTR_ERR(tcan4x5x->device_wake_gpio) == -EPROBE_DEFER)
return -EPROBE_DEFER;
tcan4x5x_disable_wake(cdev);
}
tcan4x5x->reset_gpio = devm_gpiod_get_optional(cdev->dev, "reset",
GPIOD_OUT_LOW);
if (IS_ERR(tcan4x5x->reset_gpio))
tcan4x5x->reset_gpio = NULL;
ret = tcan4x5x_reset(tcan4x5x);
if (ret)
return ret;
tcan4x5x->device_state_gpio = devm_gpiod_get_optional(cdev->dev,
"device-state",
GPIOD_IN);
if (IS_ERR(tcan4x5x->device_state_gpio)) {
tcan4x5x->device_state_gpio = NULL;
tcan4x5x_disable_state(cdev);
}
return 0;
}
static const struct regmap_config tcan4x5x_regmap = {
.reg_bits = 32,
.val_bits = 32,
.cache_type = REGCACHE_NONE,
.max_register = TCAN4X5X_MAX_REGISTER,
};
static struct m_can_ops tcan4x5x_ops = {
.init = tcan4x5x_init,
.read_reg = tcan4x5x_read_reg,
.write_reg = tcan4x5x_write_reg,
.write_fifo = tcan4x5x_write_fifo,
.read_fifo = tcan4x5x_read_fifo,
.clear_interrupts = tcan4x5x_clear_interrupts,
};
static int tcan4x5x_can_probe(struct spi_device *spi)
{
struct tcan4x5x_priv *priv;
struct m_can_classdev *mcan_class;
int freq, ret;
mcan_class = m_can_class_allocate_dev(&spi->dev);
if (!mcan_class)
return -ENOMEM;
priv = devm_kzalloc(&spi->dev, sizeof(*priv), GFP_KERNEL);
if (!priv)
return -ENOMEM;
priv->power = devm_regulator_get_optional(&spi->dev, "vsup");
if (PTR_ERR(priv->power) == -EPROBE_DEFER)
return -EPROBE_DEFER;
else
priv->power = NULL;
mcan_class->device_data = priv;
m_can_class_get_clocks(mcan_class);
if (IS_ERR(mcan_class->cclk)) {
dev_err(&spi->dev, "no CAN clock source defined\n");
freq = TCAN4X5X_EXT_CLK_DEF;
} else {
freq = clk_get_rate(mcan_class->cclk);
}
/* Sanity check */
if (freq < 20000000 || freq > TCAN4X5X_EXT_CLK_DEF)
return -ERANGE;
priv->reg_offset = TCAN4X5X_MCAN_OFFSET;
priv->mram_start = TCAN4X5X_MRAM_START;
priv->spi = spi;
priv->mcan_dev = mcan_class;
mcan_class->pm_clock_support = 0;
mcan_class->can.clock.freq = freq;
mcan_class->dev = &spi->dev;
mcan_class->ops = &tcan4x5x_ops;
mcan_class->is_peripheral = true;
mcan_class->bit_timing = &tcan4x5x_bittiming_const;
mcan_class->data_timing = &tcan4x5x_data_bittiming_const;
mcan_class->net->irq = spi->irq;
spi_set_drvdata(spi, priv);
/* Configure the SPI bus */
spi->bits_per_word = 32;
ret = spi_setup(spi);
if (ret)
goto out_clk;
priv->regmap = devm_regmap_init(&spi->dev, &tcan4x5x_bus,
&spi->dev, &tcan4x5x_regmap);
ret = tcan4x5x_power_enable(priv->power, 1);
if (ret)
goto out_clk;
ret = tcan4x5x_parse_config(mcan_class);
if (ret)
goto out_power;
ret = tcan4x5x_init(mcan_class);
if (ret)
goto out_power;
ret = m_can_class_register(mcan_class);
if (ret)
goto out_power;
netdev_info(mcan_class->net, "TCAN4X5X successfully initialized.\n");
return 0;
out_power:
tcan4x5x_power_enable(priv->power, 0);
out_clk:
if (!IS_ERR(mcan_class->cclk)) {
clk_disable_unprepare(mcan_class->cclk);
clk_disable_unprepare(mcan_class->hclk);
}
dev_err(&spi->dev, "Probe failed, err=%d\n", ret);
return ret;
}
static int tcan4x5x_can_remove(struct spi_device *spi)
{
struct tcan4x5x_priv *priv = spi_get_drvdata(spi);
tcan4x5x_power_enable(priv->power, 0);
m_can_class_unregister(priv->mcan_dev);
return 0;
}
static const struct of_device_id tcan4x5x_of_match[] = {
{ .compatible = "ti,tcan4x5x", },
{ }
};
MODULE_DEVICE_TABLE(of, tcan4x5x_of_match);
static const struct spi_device_id tcan4x5x_id_table[] = {
{
.name = "tcan4x5x",
.driver_data = 0,
},
{ }
};
MODULE_DEVICE_TABLE(spi, tcan4x5x_id_table);
static struct spi_driver tcan4x5x_can_driver = {
.driver = {
.name = DEVICE_NAME,
.of_match_table = tcan4x5x_of_match,
.pm = NULL,
},
.id_table = tcan4x5x_id_table,
.probe = tcan4x5x_can_probe,
.remove = tcan4x5x_can_remove,
};
module_spi_driver(tcan4x5x_can_driver);
MODULE_AUTHOR("Dan Murphy <dmurphy@ti.com>");
MODULE_DESCRIPTION("Texas Instruments TCAN4x5x CAN driver");
MODULE_LICENSE("GPL v2");
Thanks,
Annie