Hello,
I'm using the TPS65987DDJ and the Application Customization tool version 6.1.1. In my design there is no external SPI flash and the patch bundle is downloaded from a EC. Therefore, I'm using the PTCx commands (PTCs, PTCd, PTCc).
The PTCs and PTCd commands do not return an error code. However, the PTCc command is returning 0x42 - Patch not compatible with this version of ROM. I have attached the project file and low region patch config file in a .c array. My pinstrap settings are:
* SPI_MISO: 0
* BP_ECWait_Internal, Infinite Wait
Is the TPS65987DDJ not compatible with the patch generated from the Application Customization tool?
Thanks,
Chamira Perera.