Part Number: THVD8000
Are there any limitations on the bus voltage like 48, 24 or 12VDC?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: THVD8000
Are there any limitations on the bus voltage like 48, 24 or 12VDC?
Hello,
There are a couple of limitations related to voltage that should be considered.
One is that the DC voltage on the transmission line should not exceed the rating of the AC-coupling capacitance used. (Note too that operation at voltages near the maximum rating can result in a derating of the capacitance, so this should be considered when choosing component values.)
Another limitation relates to the ramp time of the supply. Since THVD8000 is separated from the power lines via AC-coupling capacitances, a steady-state DC voltage on the line would not stress the transceiver. However, fast supply ramps (or "hot plug" events) could result in some voltage transferring through the coupling capacitances and showing up at the device pins. For higher voltages and faster ramps, it can be beneficial to clamp the voltage at the THVD8000 interface pins using a Zener diode or TVS.
Regards,
Max