Part Number: TPS65987D
Other Parts Discussed in Thread: BQ25703, TPS65987,
I have problem with Application Customization tool and I2C3 port
I try to configure TPS65987DH I2C3 port as master and BQ25703 is slave. When I use PC with I2C tool to write BQ25703 registers and parameters the BQ25703 start up and works OK. I can Charge battery.
Same parameters written to TPS65987 Application Customization tool according to SLVAE18
I Tried to change register 5C but no success, the I2c3 port stays not active. Can't see any clk or data pulses if I use oscilloscope.
What registers need to be set to get I2c3 port activated?
What I tried was register 5C bytes 1 to 4 to get gpio 5 and gpio 6 to enabled. ( my first set was like 12C004 and then enable to bit 5 and 6 -> 12C064 )