Part Number: TPS65982
Hi,
Our device with tps65982 is configured as a dp-alt-mode source. When plugging in a dp-alt-mode adapter (that works flawlessly when attached to e.g. a Laptop with usb-c) the tps65982 negotiates DP alt mode successfully (verified by data status register 0x5f) and DP sid status (0x58) however DPStatusRX in 0x58 never changes the HPD state (Bit 7), other pars of DPStatusRX look valid. I have not used a PD analyzer.
- How can i get more debugging information why hpd is never toggled (without a protocol analyzer)?
- Is that bit solely responsible for triggering the tps65982 GPIO4 when acting as DP source ?
- Is alt lane muxing dependent on hpd status or are they already muxed after dp-alt-mode contract negotiation?
(Tried retriggering contract via `AMDs` 4cc command does not change the hpd status).
Thanks for any pointers!