Other Parts Discussed in Thread: TCAN4550
Ho all,
Is it possible to use a 6 mhz crystal? Even though I have restrictions on possible CAN baudarates, are the rest of the features operational? In particular, is the spi working with this frequency?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Ho all,
Is it possible to use a 6 mhz crystal? Even though I have restrictions on possible CAN baudarates, are the rest of the features operational? In particular, is the spi working with this frequency?
Hi Manu,
I am assuming you want to use a 6 Megahertz cyrstal (MHz) and not a 6 millihertz (mHz) crystal, if so, yes that is possible. The only restriction you will have is that the SPI frequency must be less than the Crystal frequency by about 1MHz. This is due to the clock synchronization circuitry that allows the data to cross from the digital core clock domain to the SPI clock domain without generating errors.
Therefore if you use a 6Mhz crystal, the maximum SPI frequency you could use would be approximately 5Mhz.
However on the odd chance you did want to use a 6mHz clock frequency, I don't think it would work at all because that would be too slow. But I know that is not what you meant and it was just a typo!
Regards,
Jonathan
Thanks for your answer.
'mHz' it's just a typo. I meant MHz.
I have to look for what the problem is, in fact on the crystal pins I have 1.2V fixed and the crystal does not seem to generate the clock. After about 4 minutes in the same pins i found 0V. Do you have any ideas that can help me diagnose and solve the problem?
Thanks in advance.
Hi Manu,
Regarding your first question about the crystal not oscillating, there may be a voltage issue, or schematic/component issue. If you would send me the schematics I can review them and look for any errors or adjustments that may be needed. If you can share them on this forum that would be great, but if you would prefer to not share them publicly, let me know and I will send you an email. But check the following:
Regarding your observation of the 0V after 4 minutes, this is an easy one and the result of a device feature. The TCAN4550 has a Failsafe Feature with 3 mechanisms that can cause the device to enter Sleep Mode which effectively turns off the device. Refer to sections 8.4.2 and 8.4.5 of the datasheet for more information. But what you are seeing is the Sleep Wake Error Timer timing out.
Upon power up, a power on reset or wake event from sleep mode causes the TCAN4550 to enter standby mode. This starts a four minute timer, tinactive, that requires the processor to either reset the interrupt flags or configure the device to normal mode. This feature makes sure the node is in the lowest power mode if the processor does not come up properly. This automatic mode change also takes place when the device has been put into sleep mode ad receives a wake event, Wake Up Pattern (WUP) on the CAN bus, or Local Wake Up (LWU) event on the WAKE pin. To disable this feature for sleep events register 16'h0800[1] (SWE_DIS) must be set to one. This will not disable the feature when powering up or when a power on reset takes place.
So, during your initial development, I recommend you disabling this feature since you will be having long delays while you run tests on the various features. You will have to disable this feature through SPI every time you power on or reset the device since this feature is enabled by default and the registers are volatile and do not retain their values when not powered. Or you can configure the device to Normal Mode within 4 minutes. If the device does go to sleep, all you need to do is toggle the WAKE pin to wake it back up. However, the register values will have also been reset.
Regards,
Jonathan