Part Number: DP83620
Other Parts Discussed in Thread: TS3L4892,
Hi Sir/Madam,
What will be the status of the TD+/TD- and RD+/RD- pins during power off condition? We are using the two DP83620 part along with the TS3L4892 switch for Pass through function (connecting two RJ45 port or connecting the each RJ45 port with its respective Ethernet PHY).
The TS3L4892 switch will be in on condition when the DP83620 is in off condition to enable pass through function. During this condition the Switch will be configured by default to connect the two RJ45 ports together disconnecting the Ethernet Phy from RJ45 ports. We want ensure in this condition there is no current flow from TS3L4892 to DP83620 which can damage the Ethernet PHY. Will the TD+/TD- and RD+/RD- pins be in High Impedance state during off condition.
Regards,
M Amarnath