Part Number: DS90UB940-Q1
Hi All,
I have a question about FPD-Link3 from LVCMOS/LVDS to mipi-csi2.
Connect DS90UB925-Q1 and DS90UB940-Q1 to convert from LVCMOS to mipi-csi2.
In this case, is RGB24-bit transmission possible?
I read " 7.3.8.1 GPIOx and D_GPIOx Pin Configuration " .
When using GPIO, RGB18bit transmission is possible.
Is it possible to use GPIO when input to RGB24bit?
Also, are there any other restrictions setting for connect LVCMOS to mipi-csi2?
I am also thinking about converting from LVDS to mipi-csi2.
In that case, connect DS90UB927-Q1 and DS90UB940-Q1.
Are there any restrictions on using GPIO with this configuration as well?
Best Regards,
Ishiwata