Part Number: DP83867E
Hi Team,
There are several threads on XI input specification topic, however,
I have several questions. Can you advise me on my question related to
the specifications for the XI of the DP83867E
I am designing Ethernet board using DP83867E and has question bellows:
Q1 The datasheet has two parameters for the XI input
They are VIH/VIL and VOSC.
I am feeling that they are contradicting each other.
Referring VIH/VIL, the delta is 0.95V.
In contrast, VOSC requires 1.4V as the minimum.
Can you let me know which parameters I should follow?
Q2. VDDIO can be selected among 1.8V, 2,5V and 3.3V.
XI parameters, VIH/VIL and VOSC can be utilized under these supply conditions?
Q3. When XI is driven from 3.3V LVCMOS, AC coupling is recommended.
Why the AC coupling is recommended instead of DC coupling with resister divider network?
I don't thins 500 ohm of resisters does not make clock edge slow.
Q4. When 3.3V LVCMOs source with two 27 pF capacitor divider is used, the minimum VOSC of 1.4V
cannot be satisfied.
3.3V LVCOS Vol <0.4V and VOH>3.3-0.4V, Delta =2.5V divide by 2 = 1.25V
How do you deal it?
Q5. When Xi is used in AC coupling mode, IX seemed to be biased VDDIO/2.
If VDDIO=1.8V, the bias level may be 0.9V.
Under this circumstance, maximum VOSC is applied to Xi, negative peak voltage
may be 0V.
If bias level validate some degrees, and 60-40% of duty cycle distortion clock is applied to
XI, the negative peak may hit the -0.3V which is the absolute maximum ratings.
Can you use the device under reliable conditions?
Mita