This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Laser diode driver



Hello,

For an illumination application i want to build a laser with a laser diode. Pulses with a width of 400ps or shorter are necessary. The repetition rate of the pulses will be about 80MHz. For the needed spectral range a 405nm diode or a red laser diode is necessary. The operating voltage is about 4.75V for the blue and 2.32V for the red diode. Will it be possible to use such a diode with a TI laser diode driver (e.g. the ONET1101L).

Regards

Bernd Widzgowski