Hello! I got a problem about the data transmission between two 1394 devices. The PHY chip is TSB81BA3E and the LLC is TSB82AA2.
All of them are from TI. And the problems are shown in the pictures below. We can see the 1394 device is installed sucessfully in the PC. We connect the two 1394 devices by a 1394b cable, howerver there is no data transmission. It seems like the link between two devices is failed or the link of PHY and LLC is failed. How can I solve the problem?
Thanks for your help!