Other Parts Discussed in Thread: DS92LV3242, DS92LV3241, SN75LVDS83B, TFP410, TFP401
We have an application to support an LCD type display some short distance from our video controller. Video is 32 bits, 1080P, 1.8V and I was considering use of the DS92LV3241/DS92LV3242.
A colleague pointed out that our video data is DDR (double data rate) and because the DS92LV324SDR/DS92LV3242 is a SDR (single data rate) device it will not work for this application.
I have two questions:
1. Can someone please suggest a DDR LVDS SERDES that might be a good choice for this application ?
2. Is there a simple solution to use the DS92LV324SDR/DS92LV3242 in a DDR application ? I would think it's only a matter of doubling the clock at the tx side, and dividing the clock by 2 at the RX side. What would be the concerns with doing this ?
Thanks a lot