I have a circuit with the TUSB2036 IC. I am able to connect to a computer and the computer recognizes the device as a generic USB hub. My problem is that after 7.6 seconds, the suspend pin goes high and the crystal stops oscillating. When I look through the datasheet and other post on the forum, most of the solution seems to be the timing of the reset circuit. I am using a 150k resistor with a 1uF cap. What possibilities would make this shut off after 7+ seconds of operation?