Currently working on debugging a design using the DP83848. I have checked all the relevant voltages at the various pins on the device and they are all correct. One thing I have discovered is we have missed off the magnetics - so I am planning on changing the existing RJ45 connector to a connector with integrated magnetics to see if this is the reason I have no activity. Can anyone advise on the most suitable integrated magnetics connector. We are not using PoE.
As our application does not need EMI fingers this cuts down the choice to J0011, J00-0014 AND J0026 options - so what will the different schematics J0011 and J0026 give?
Also - no activity on MDC and MDIO lines - and TX_EN is sitting about 0.4V.
PFBOUT and PFBIB1,2 voltages are correct.
25MHz clock is present
RBIAS is correct at 4K87
MDIO pull-up resistor is correct at 1K5
RESET_N is sitting High