Other Parts Discussed in Thread: TUSB9261
I'm working on a project with the TUSB9261 using the default firmware, v1.05, and I am experiencing problems trying to get it to connect with my computer as a hard drive. It had no problems communicating with the computer in bootloader mode and flashing the firmware. In the UART output I get the following when I connect power and then plug in the USB:
========================================================
|| TUSB926x Firmware v1.05 [Oct 3 2014 16:33:57] ||
|| Device ID: 0x0000 ||
========================================================
Reset Flag(s): [Power-Up]
[0000000001] Datapath RAM Usage: 80208 / 81920 bytes.
[0000000001] Supported NCQ Depth: 32
[0000000001] U1/U2 Transistions: OFF
[0000000001] USB PHY Suspend: ON
[0000000001] SATA LPM: OFF
[0000000001] Device is Bus-powered.
[0000000001] -> usb_hal_init()
[0000000001] USB Core Ver: 0x120a.
[0000000001] USB SSC is OFF.
[0000000051] -> usb_hal_connect()
[0000000051][0000000051] LTSSM state = (0x5) RX DETECT.
-> ahci_init()
[0000000051] -> ahci_hba_reset()
[0000000056] SATA Gen-2 speed negotiated.
[0000000150] HS/FS/LS state = (0x0) ON.
[0000000153] HS/FS/LS state = (0x5) EARLY SUSPEND.
[0000000156] HS/FS/LS state = (0x3) SUSPEND.
[0000002973]
[0000002973] ================================================
[0000002973] IDENTIFY DEVICE INFO
[0000002973] ================================================
[0000002973]
[0000002973] Model: WDC WD1600BEKT-66F3T2
[0000002973] FW Rev: 13.01A13
[0000002973] Serial: WD-WX80AA9H6844
[0000002973]
[0000002973] Spec Compliance: ATA-7
[0000002973] Removable Media: No
[0000002973] Rotational Speed = 7200 RPM
[0000002973] UDMA Modes = 0x003f
[0000002973] PIO Modes = 0x0003
[0000002973]
[0000002973] LBA48: Yes
[0000002973] Max LBA = 0x00000000 12a19eb0
[0000002973] Write FUA: No
[0000002973] World Wide Name = 0x50014ee2 03a7cf2b
[0000002973]
[0000002973] SATA Speed: Gen2
[0000002973] NCQ Support: Yes
[0000002973] Queue Depth = 31
[0000002973]
[0000002973] Logical Sector Size = 512 bytes
[0000002973] Physical Sector Size = 512 bytes
[0000002973] Logical Sector Offset = 0
[0000002974]
[0000002974] ================================================
[0000002977] Connected to 1 AHCI device(s).
[0000049047] Num of port resets = 6.
[0000049047] USB Reset event occurred.
[0000049047] -> ahci_reset_lun(0)
[0000049047] -> ahci_fatal_error_recovery() - dev_status = 0x00000080, outstanding_cmd_slots = 0x00000000, force_comreset = 0.
[0000049047] -> ahci_port_reset(0)
[0000049522] Connected at HIGH speed.
[0000049522] HS/FS/LS state = (0x0) ON.
[0000049522] -> gio_isr() - flags = 0x00000008.
[0000049522] Push button input detected.
[0000050025] HS/FS/LS state = (0x5) EARLY SUSPEND.
[0000050026] USB Reset event occurred.
[0000050026] -> ahci_reset_lun(0)
[0000050037] Connected at HIGH speed.
[0000050037] HS/FS/LS state = (0x0) ON.
[0000050054] -> usb_hal_set_address() - addr: 0x9.
[0000050082] -> handle_usb_set_configuration() - val = 1.
[0000050104] AHCI task file error! P0TFD error = 0x04, status = 0x51.
[0000050104] -> ums_bot_ata_error_callback() - gBOT_state = 3.
[0000050104] -> ums_bot_send_CSW() - status = FAILED. CDB[0] = 0xa2.
[0000050105] AHCI task file error! P0TFD error = 0x04, status = 0x51.
[0000050105] -> ums_bot_ata_error_callback() - gBOT_state = 3.
[0000050105] -> ums_bot_send_CSW() - status = FAILED. CDB[0] = 0xa2.
[0000050105] AHCI task file error! P0TFD error = 0x04, status = 0x51.
[0000050105] -> ums_bot_ata_error_callback() - gBOT_state = 3.
[0000050105] -> ums_bot_send_CSW() - status = FAILED. CDB[0] = 0xa2.
[0000050105] AHCI task file error! P0TFD error = 0x04, status = 0x51.
[0000050106] -> ums_bot_ata_error_callback() - gBOT_state = 3.
[0000050106] -> ums_bot_send_CSW() - status = FAILED. CDB[0] = 0xa2.
[0000050106] AHCI task file error! P0TFD error = 0x04, status = 0x51.
[0000050106] -> ums_bot_ata_error_callback() - gBOT_state = 3.
[0000050106] -> ums_bot_send_CSW() - status = FAILED. CDB[0] = 0xa2.
[0000050106] AHCI task file error! P0TFD error = 0x04, status = 0x51.
[0000050106] -> ums_bot_ata_error_callback() - gBOT_state = 3.
[0000050106] -> ums_bot_send_CSW() - status = FAILED. CDB[0] = 0xa2.
[0000050107] -> ums_bot_case_handler() - case 5.
[0000050107] -> ums_bot_case_handler() - case 5.
[0000050133] @Warning: scsi_handle_mode_sense_cmd() - page code 0x1c not supported.
[0000050133] -> ums_bot_send_CSW() - status = FAILED. CDB[0] = 0x1a.
[0000050133] -> ums_bot_case_handler() - case 5.
[0000050134] -> ums_bot_case_handler() - case 5.
[0000050134] -> ums_bot_case_handler() - case 5.
[0000050137] -> ums_bot_case_handler() - case 5.
[0000050139] -> ums_bot_case_handler() - case 5.
[0000050210] -> ums_bot_case_handler() - case 5.
[0000050210] -> ums_bot_case_handler() - case 5.
[0000050230] -> ums_bot_case_handler() - case 5.
[0000050230] -> ums_bot_case_handler() - case 5.
[0000050250] -> ums_bot_case_handler() - case 5.
[0000050250] -> ums_bot_case_handler() - case 5.
[0000050254] -> ums_bot_case_handler() - case 5.
[0000050254] -> ums_bot_case_handler() - case 5.
[0000050258] -> ums_bot_case_handler() - case 5.
[0000050258] -> ums_bot_case_handler() - case 5.
[0000050277] -> ums_bot_case_handler() - case 5.
[0000050278] -> ums_bot_case_handler() - case 5.
[0000050296] -> ums_bot_case_handler() - case 5.
[0000050296] -> ums_bot_case_handler() - case 5.
Where do I find the interpretation of these errors? Is there documentation for the Firmware itself?
Also, how do I configure the system to run the HDD solely from USB 2.0 or greater?
Thanks,
Aaron