Other Parts Discussed in Thread: TCAN1042-Q1
Hello,
I'm looking for a way to completely disable the CAN transceiver TCAN1042-Q1. Here "completely disable" means, the device won't wake up an external MCU by WUP (Wake Up Pattern) AND the device won't transmit a signal from the MCU onto CAN bus.
- As long as the transceiver stays in standby mode by enabling its STB pin, the TXD pin won't accept any signal.
- Idea 1: If a gate logic is placed between the RXD pin and the MCU, I guess it can block a signal triggered by WUP. But, will it activate the transceiver too and will a signal on the TXD pin be transmitted onto the CAN bus?
- Idea 2: V-suffix versions integrate a level shifter. If a VIO pin is tied to GND, will it prevent a signal triggered by WUP from coming out from the RXD pin? If yes, is there any possible current leakage path between VIO and VCC pins when the VIO is at GND while the VCC is on?
Any other ideas?
Best regards,
Shinichi Yokota