Part Number: SN65DSI84
Hi everyone,
I am working on a design based on this mipi-lvds bridge to drive either a 1280x800 10" lcd or a 1024x600 7" lcd. The video source is an Intel Atom x5-Z8350 cpu on an Upboard SBC.
My problem is that the bridge works well when the 1280x800 resolution is selected in the BIOS but not with the 1024x600.
Hardware
- Two DSI channels (DA0-DA1) and only LVDS channel A are used.
- The DSI clock is not used since we couldn't enable it on the cpu.
- An external refclock is provided by an oscillator of 25MHz (7" LCD) or 35MHz (10" LCD).
Configuration
- Configuration has been generated with TI's DSI Tuner.
- The DSI source is 24bbp.
- The REFCLK_MULTIPLIER register is set at 2 to generate the 50MHz and 70MHz LVDS clock needed by the displays.
- Panel inputs and DSI inputs have been verified using the LCD datasheets and the video BIOS settings.
- Related registers are configured for either the 25MHz or 35MHz refclock.
Results
- The 10" configuration is working on the 10" LCD and the 7" LCD (works with 7" LCD even if the LVDS clock is higher than specified in the display's datasheet).
- The 7" configuration is not working; LVDS lanes Y1 and Y3 seem to be dc biased but have no activity on them.
- Both the 50MHz and 70MHz LVDS clocks are generated successfully by the sn65dsi84.
- When the refclk is provided by an externel frequency generator set to 50MHz and having REFCLK_MULTIPLIER set to 1, the LVDS clock looks fine but still nothing on Y1 and Y3.
- If the test pattern is activated (register 0x3c) with the 7" configuration, the display is white with a black border.
Both DSI tuner configurations are attached.
Any insight on what could be wrong and what should be further tested would be greatly appreciated.
Thank you,
Charles
%CHIP2%PVCAHKSebo New Display Co%PMCANDS7G50PIPS-3.5%RPCA1024%RLCA600%PVCB%PMCB%RPCB%RLCB%LVCM0%HPWA20%HBPA140%HFPA160%HACA1024%HTOA1344%HPWB%HBPB%HFPB%HACB%HTOB0%VPWA3%VBPA20%VFPA12%VACA600%VTOA635%VPWB%VBPB%VFPB%VACB%VTOB0%PCKN51.2%LCKS1%RCKM25%MULT1%DCKA%DIVI3%LCKR50.0%FMTA1%DEPA0%HSPA1%VSPA1%BPPA1%FMTB1%DEPB0%HSPB1%VSPB1%BPPB0%PRDA1024x600%PRDBx%DSCM0%LREO1%LRCE1%LPCA0%BMCA1%SMCA1%LPCB0%BMCB0%SMCB0%DHPA112%DHBA40%DHFA168%DHAA1024%DHTA1344%DHPB%DHBB%DHFB%DHAB%DHTB%DVPA29%DVBA1%DVFA5%DVAA600%DVTA635%DVPB%DVBB%DVFB%DVAB%DVTB%DDRA51%NOLA1%VIMA2%LCRP%DDRB%NOLB0%VIMB0%RCRP
%CHIP2%PVCAHKSebo New Display Co%PMCAYX101IA-01G%RPCA1280%RLCA800%PVCB%PMCB%RPCB%RLCB%LVCM0%HPWA80%HBPA0%HFPA40%HACA1280%HTOA1400%HPWB%HBPB%HFPB%HACB%HTOB0%VPWA10%VBPA3%VFPA10%VACA800%VTOA823%VPWB%VBPB%VFPB%VACB%VTOB0%PCKN71.1%LCKS1%RCKM35%MULT1%DCKA%DIVI3%LCKR70.0%FMTA1%DEPA0%HSPA1%VSPA1%BPPA1%FMTB1%DEPB0%HSPB1%VSPB1%BPPB0%PRDA1280x800%PRDBx%DSCM0%LREO1%LRCE1%LPCA0%BMCA1%SMCA1%LPCB0%BMCB0%SMCB0%DHPA32%DHBA48%DHFA80%DHAA1280%DHTA1440%DHPB%DHBB%DHFB%DHAB%DHTB0%DVPA10%DVBA3%DVFA10%DVAA800%DVTA823%DVPB%DVBB%DVFB%DVAB%DVTB%DDRA71%NOLA1%VIMA2%LCRP%DDRB%NOLB0%VIMB0%RCRP