Part Number: SN65DP141
Other Parts Discussed in Thread: TUSB546-DCI
Team,
I have seen the below post already which gives some useful information:
https://e2e.ti.com/support/interface/digital_interface/f/130/p/533872/1949167#1949167
Do we have some more precise guidelines regarding the settings of the Equalization mode and RX Gain?
-Section 8.4.2 to 8.4.3 lists some possible GPIO mode settings.
-Section 8.4.4 lists possible settings via I2C mode and respective application
http://www.ti.com/product/SN65DP141/datasheet/detailed-description#sllses62960
Q:I assume that the GPIO and I2C settings are a one to one match. correct?
Q:Do we have more precise info on what we mean by Short/Long Input Cable and small/Large Input Swing.
Could you quantify it?
The idea is to have a GPIO mode setting that covers the most probable scenario so that the I2C mode does not need to be used.
In the current scenario there is:
Connector -> DP141 ->trace (of a couple of cm) -> FPGA
The DP141 should enable to recover the signal coming from a long cable. Still it should work as well in case cable are short.
Thanks in advance,
Anthony