This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB953-Q1: MIPI RAW20 support

Guru 20090 points

Part Number: DS90UB953-Q1

Hello,

Can we use DS90UB953-Q1 and 954-Q1 for MIPI RAW20 format?
There is similar post but the reply was done offline.

Pixel: 1.3Mpix (1344 * 968)
Frame Rate: 30fps
Format: RAW20
Mbps/Lane : 750Mbps

Best Regards,
Ryuji

  • Yes, the DS90UB953-Q1 will support RAW20 format. The 953 will pass through the mipi packets as received and as long as the datarate and throughput is within the capability of the 953 and deserializer any type format can be supported.