Hi,
I'm using the TCA9617B as a level shifter between Aardvark (3.3V level) to a Slave device (1.8V level).Since side B can't support 1.8V level I connected the Slave device to Side A and the Master device to Side B.Is it a valid connection? What would be the recommanded typical pull-up resistors for using 800K speed?
Regards,
Matty