Other Parts Discussed in Thread: TPS2042
Hi all!
I've been facing an issue regarding to the TUSB2046B USB HUB. The PCB I have developed is attached to the USB Port of the RPI-Zero.
When i start the device, it seems the 5V is running smootly, 3V3 regulator also works. After 2-4 seconds after power-up I do see 5V on the USB outputs (USB1_5V and USB2_5V), I'm asuming the TUSB2046B and TPS2042 is starting up correctly then? Or am I missing something?
A side note: when i disconnect the RPI-Z, it seems not to be starting up? Do i need the Upstream USB0_DM and USB0_DP in order to activate the device?
When I connect a simple keyboard to the hub it doesn't get recognized I don't see anything happening when I press a key on my keyboard. When I attach the Keyboard directly to the RPI-Z I can type anything, that seems to work, but not with the USB-Hub.
I've already changed some few things:
- Add & Remove the 1K5 pull-up resistor on the USB_DP0 (R1)
- Add & Remove the 1K5 resistor (R19/R20) to XTAL2 (placed a solder bridge instead)
- Removed the 15K pull-up resistor to OC1 & OC2 (R15 & R16)
- Changed the 18pF (C11 & C12) to 27pF.
Where does it goes wrong? Is my schematic correct? It's based upon the provided reference schematic on the TI website.
thanks for any help in advance!
Best regards,
Klaas de Boer | Embedded System Engineer | KEY Electronica