Part Number: SN65HVD234-Q1
Thanks in advance for any help.
I just created a new design using the 3.3v transceiver coupled with an MCP2515.
Everything works fine with the MCP2551 (at 5 volts) with the MCP2515 at 3.3v on the bench.
My new design doesn't have 5v which is why I ordered this chip. I swap them out changing the rail voltage to 3.3v which what the is MCP 2515 is using (yet it doesn't function).
My current wiring for Both chips (On bread board before I waste my circuit boards) is:
Pin 1 - TXD
Pin 2 - GND
Pin 3 - 3.3v (5 volt when using MCP2551)
Pin 4- RXD
Pin 5 - 3.3v
Pin 6 - CAN L
Pin 7 - CAN H
Pin 8 - GND
I have checked voltages while running and getting 3.2 volts. When I swap back MCP and change rail to 5v it works fine. So I don't think there is any issue with the other connections.
There are no other resistors hooked up at the moment other then 120 ohm between CANH and CANL
I'm verifying output with a Kvaser Leaf CAN sniffer.
Am I missing something? I thought this chip would be a direct swap for the MCP with the exception of voltage.
I've also tried 2 different new transceivers with same results.
Please help...
David