Part Number: TUSB2046B
Team: Customer have produced thousands of boards in different products using the TUSB2046BVF. While testing a new run of boards with the same parts and board design that has worked in over 100 shipped products, they are now getting a "USB Device Not Recognized" error whenever the USB cable is plugged in to the product. In Device Manager, the USB Hub is showing, the HID-compliant device for our application, and one Unused Port. Two other unused ports on the hub are showing as "Unknown USB Device" and giving an error. The pins on the chip for the two unused ports are not brought out to connect to anything.
The error will be an issue for our customers and create customer calls. I can send screen caps of the error and the schematic. Please advise. Thank you.