This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867E: JTAG interface timing

Part Number: DP83867E


Hello, I am working with a design that is concerned with the timing of the JTAG interface on the DP83867E.

We wer able to obtain the below info:

JTAG_TDO: setup 2ns, hold 1.5ns

JTAG_TDI/TMS: setup 5ns, hold 2ns.

We were also able to use the IBIS model to uncover what the  high to low propagation delay (tPHL) and the low to high propagation delay (tPLH) for the JTAG signal was but an addition question we have is below:

-What is the clock to TDO skew in regards to the JTAG interface? Also, what is the clock to TDI skew in regards to the JTAG interface?

I could not find the info in the datasheet, is the information available, did I miss it?